Cancel
Showing results for 
Search instead for 
Did you mean: 

New to Teamcenter - Good examples of setting up a basic workflow?

Experimenter
Experimenter

I'm a professor at Purdue and I'm attempting to introduce Teamcenter to my 200 level class this semester for the first time.'

 

I'm trying to setup a *very* basic workflow so that the students can check a file in and then set to to a status so that the TA or I can review it.  So far I haven't found any good easy to understand documentation on workflows (at least for a newbie) or what the OOTB configurations do and which roles the tasks are routed to. Can anyone point me in the right direction?

 

Thanks.

1 REPLY

Re: New to Teamcenter - Good examples of setting up a basic workflow?

Genius
Genius

Hello Professor,


There is a lot of documentation available on GTAC (Global Technical Access Center) website. You would need to obtain an Webkey account to access it.


Please click on on the below link to read / know about the workflows in Teamcenter, There are also couple of good examples avaliable.


https://support.industrysoftware.automation.siemens.com/docs/teamcenter/10.1.3/help/#uid:index_workf...


Hope this helps !

Thanks,

Teamcenter 10.1.7
TC Visualization 10.1.7
NX:11.02 | NX 9.02 | Catia V5 R2012 | AutoCAD 2018 | In-Context Editor |