Cancel
Showing results for 
Search instead for 
Did you mean: 

Notifying Users based on the Item Types

Genius
Genius

Hello,

 

I was wondering, if there is a way to achieve this following through the configuration in TC 10.1.3

 

Business Case: We have two different item types, which goes through the same workflow process for the review. But would like to notify different groups based on the Item type.

 

Item Revision Type A >> Workflow 1 >> On completion notify >> Group X

Item Revision Type B >> Workflow 1 >> On completion notify >> Group Y.

 

PS: Checked if i can achieve this through subscriptions, but i could not find an event for release / assign status.

 

Can someone give pointers ?

 

Cheers!

 

 

 

Teamcenter 10.1.7
TC Visualization 10.1.7
NX:11.02 | NX 9.02 | Catia V5 R2012 | AutoCAD 2018 | In-Context Editor |
2 REPLIES

Re: Notifying Users based on the Item Types

Legend
Legend

Take a look at the thread - Sending notification on release of Item.

 

It is not exactly same as your questions, but the solution will fit your need quite well.

---

Thanks and Regards

Yogesh Fegade

Re: Notifying Users based on the Item Types

Genius
Genius

Thank you for the response. but our workflow has some customisation after statusing and cannot include additional conditional task.

 

Will be achieving this thru the customisation itself.

 

Cheers !

 

Teamcenter 10.1.7
TC Visualization 10.1.7
NX:11.02 | NX 9.02 | Catia V5 R2012 | AutoCAD 2018 | In-Context Editor |