Cancel
Showing results for 
Search instead for 
Did you mean: 

Nx not opening files from local cache

Experimenter
Experimenter

Hi,

 

I am new to Teamcenter and NX integration. 

 

We have completed the integration and there is no error. 

The issue I am facing is of very high load times of models when it is opened in Nx.

It looks like the files are loaded from the client server instead of the local cache. The network speed is about 40mbps.

 

We are not able to resolve this issue.

Please help.

 

Thanks

Jacob

9 REPLIES 9

Re: Nx not opening files from local cache

Siemens Creator Siemens Creator
Siemens Creator

 

Can you give more detail? 

 

NX should first try to open from the FCC; your FCC defaults in the FMS master should be increased to 8GB (vs 1GB which is default).  It sounds like you also have a local FSC, check to ensure you have the proper cache size set up as OOTB it does not actually set a cache size .  See below from FMS master and FSC config, if in your FSC config you have zero extent files you are not actually server side caching.  Use the FMSCacheSizingTool_Ver_1_3.xlsx to determine your cache settings,  Would guess you should start with 20GB Read and 10 Write.

 

FCC defaults in FMS Master

      <property name="FCC_MaxReadCacheSize" value="8000M" overridable="true" />
      <property name="FCC_MaxWriteCacheSize" value="8000M" overridable="true" />

 

FSC Config: ensure that you are actually server side caching, if set like below then you have no server side cache.

    <property name="FSC_MaximumReadCacheExtentFiles" value="0" overridable="true" />
 

 

 

Re: Nx not opening files from local cache

Legend
Legend

40Mb/s - it's your total channel bandwidth? So it could be not enouth if many clients working.

Re: Nx not opening files from local cache

Creator
Creator
Where to find this particular file:
FMSCacheSizingTool_Ver_1_3.xlsx?

Re: Nx not opening files from local cache

Siemens Creator Siemens Creator
Siemens Creator

You can find it on the GTAC download site: https://download.industrysoftware.automation.siemens.com under Teamcenter, Product Updates, Tools.

Re: Nx not opening files from local cache

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
TC_ROOT\fsc\bin

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Nx not opening files from local cache

Creator
Creator

Thank You! I didnt know it was there. It's a useful guide and tool hidden out there.

Re: Nx not opening files from local cache

Experimenter
Experimenter

@Commander wrote:

 

Can you give more detail? 

 

NX should first try to open from the FCC; your FCC defaults in the FMS master should be increased to 8GB (vs 1GB which is default).  It sounds like you also have a local FSC, check to ensure you have the proper cache size set up as OOTB it does not actually set a cache size .  See below from FMS master and FSC config, if in your FSC config you have zero extent files you are not actually server side caching.  Use the FMSCacheSizingTool_Ver_1_3.xlsx to determine your cache settings,  Would guess you should start with 20GB Read and 10 Write.

 

FCC defaults in FMS Master

      <property name="FCC_MaxReadCacheSize" value="8000M" overridable="true" />
      <property name="FCC_MaxWriteCacheSize" value="8000M" overridable="true" />

 

FSC Config: ensure that you are actually server side caching, if set like below then you have no server side cache.

    <property name="FSC_MaximumReadCacheExtentFiles" value="0" overridable="true" />
 

 

 


Thank you for the reply.

 

I will check this and revert back. 

 

What additional details you would need?

 

Thanks

Jacob

Re: Nx not opening files from local cache

Experimenter
Experimenter

40 mbps is available for one workstation.

Re: Nx not opening files from local cache

Siemens Creator Siemens Creator
Siemens Creator

 

Just more details on deployed architecture, secondary cache servers and size config details of FSC XML, etc.