Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

OOTB Duplicate issue resolved

Experimenter
Experimenter

Hello Team,

 

FYIP...

Recently we have come across issues with the OOTB Duplicate function in teamcenter 11.2.2

 

Problem :  Error message displayed when executing Duplicate on a Design revision from Structure manager

 

Structure::cloneStructure(): UGS::Error::Exception
SS_CFI_path given NULL or empty path name 000000B1919F0CB8 (Error Code: 65) (2)
UGPART-ATTR
UGPART-BBOX
UGPART-ATTRIBUTES
UG-QuickAccess-Text
UG-QuickAccess-Binary
UGPART
Dataset D103638-A has 6 references
The named reference "APPUID-OBJ" cannot be added to the Dataset, because the reference does not exist.
File already exists
Please see the log file 'E:\Logs\Teamcenter\TcServer\tcserver.exe683cc890.syslog' on the server '' for more information

 

 

 

Solution
          Set the Teamcenter preference "Enable_Server_Image_Processing" to "False"

         

This preference enables the thumbnails functionality, which converts all
images associated with Item Revisions to small thumbnail images that are
displayed in the Preview area of the Summary tab, in the header of the Summary
page, and in the search results.

 

Administrators must perform multiple configurations to enable thumbnails 

functionality (see "Getting Started with Document Management" chapter in the
technical documentation). Performance and resource implications must also be
assessed.

 

Valid values are:
* true: Enables server processing of images to generate thumbnail datasets.
* false: Disables server processing of images to generate thumbnail