Cancel
Showing results for 
Search instead for 
Did you mean: 

OTW on .NET

Valued Contributor
Valued Contributor

Dear Listers,

 

We have an .NET setup of Teamcenter with Middle Tier on .NET and Webtier on .NET.  Would like to know if any one has done the OTW implementation on .NET( Middle Tier and Web-Tier ). IF there are any documents on this , please advise.

 

Regards

Vilas

6 REPLIES

Re: OTW on .NET

Phenom
Phenom

Good afternoon, maybe you are looking for this:

https://support.industrysoftware.automation.siemens.com/docs -> Teamcenter -> Teamcenter 11.4 Product Documentation – PDF-> Teamcenter Installation ->  Windows Server Installation

Teamcenter Installation on Windows Servers

Chapter 9 .NET Web tier installation

Chapter 11 Installing the server manager -> Install the .NET server manager

Re: OTW on .NET

Valued Contributor
Valued Contributor

Hi Arthur,

 

Thanks for the reply. We have successfully installed the .NET server manager and .NET web tier. Would like to know th procedure to setup OTW on a .NET setup.

If there are any documents kindly help us.

 

Regards

Vilas

Re: OTW on .NET

Phenom
Phenom

You must do what is written in

10 J2EE Web tier installation

Install the Web Application Manager -> Installing rich client Web applications

The difference will be in your web server,
for .NET IIS is used

iis.png

Re: OTW on .NET

Phenom
Phenom

Addition, after installation WAM:

Created a new directory under the 'tc' virtual directory in IIS called
'otwdev' and copied the content of the
% DISTRIBUTION_SERVER_INSTANCE% \ webapp_root \ otwweb to that location.

Client Side:
1. Navigated to the new OTW URL of http: //hostname/port/tc/otwdev/otw.html to
begin the OTW installation.

2. Upon running the OTW RAC, it is noticed that the URL name is not desired.
Go back to the server and update the HTTPServerTable in INSWEB to the proper
desired name and also update the URL for the Teamcenter app server.

3. Re-run the OTW RAC, it updates and now the RAC shows the values desired.

This should allow login via the OTW RAC.

* The use of 'otwdev' is not a required folder name. Use of this name here is
an example.

Re: OTW on .NET

Valued Contributor
Valued Contributor

Hi Arthur : Thanks for the inputs. Will try this and keep you posted.

 

Regards

Vilas

Re: OTW on .NET

Solution Partner Honored Contributor Solution Partner Honored Contributor
Solution Partner Honored Contributor
After installing INSWEB and loading the OTW ICD's (for example Tc11.2.0_otw.zip), you will not need the "Web_tier" ICD's since these are for tc.war, then you can create the Distribution Server and Distribution Server Instance.

The Distribution Server consists of two processes: RMI and Distribution Server. You can run them manually in a command window or turn them into services.

The Distribution Server Instance, which is actually the 4tRAC. This is the part that you will direct the IIS virtual directory as described by @ArthurRM.
Note: you can install features but you cannot uninstall instead, delete and create again.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4