Cancel
Showing results for 
Search instead for 
Did you mean: 

Open in Solid Edge ST10 and Active Workspace 3.3.2

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

I want to integrate hosted AWC with SE ST10.

I did all instructions.

AWC is showing in SE.

But I can't force AWC to show "Open in Solid Edge" button:)

 

SEEC admin is saying

2017-09-14_21h11_10.png

 

All set and still nothing...

 

From server site I have SEEC template already imported and general SE<->TC integration work's.

I see there under Active workspace dir, NX integration / Client but no Solid Edge:).

Do I need to install special feature to AWC?

Where to get it?

6 REPLIES

Re: Open in Solid Edge ST10 and Active Workspace 3.3.2

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi,

I had similar problem, and I added this values to AWC_SEEC_OpenSupportedTypes:

SE Assembly

SE Part

SE Draft

SE SheetMetal

SE Weldment

Item

ItemRevision

Also when you install client you have to choose MCAD Integration. But If you add those values it should work.

Maybe you will have to update AWC client settings after this.

Re: Open in Solid Edge ST10 and Active Workspace 3.3.2

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

MCAD Integration

 

This was key;)

Re: Open in Solid Edge ST10 and Active Workspace 3.3.2

Valued Contributor
Valued Contributor

Hi,

 

I am facing right now with the similar issue 

 

When tem.bat launch, I see MCAD integration is not selectable. Is there some different procedure to 

install it?

 

 image.png

Regards
Rafa

Re: Open in Solid Edge ST10 and Active Workspace 3.3.2

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Be shure that you run tem as administrator (or disable UAC [preffered])

 

I have selected features as dectribed here:

 

Just add mcad:

 

Re: Open in Solid Edge ST10 and Active Workspace 3.3.2

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Hover over the feature "MCAD Integration" to see what the requirements are or you may need extra licensing.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Open in Solid Edge ST10 and Active Workspace 3.3.2

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Indeed;)