Cancel
Showing results for 
Search instead for 
Did you mean: 

Opening Items with NX dataset in Solidworks with SWIM

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Hi guys.

I can open items created with Solidworks Integration under NX without problems.
How can I donthe opposite?
How can I open an NX created item inside Solidworks using SWIM?
Is this possible?

Cem
4 REPLIES

Re: Opening Items with NX dataset in Solidworks with SWIM

Solution Partner Honored Contributor Solution Partner Honored Contributor
Solution Partner Honored Contributor

You might be able to open a JT but you cannot directly open NX in SolidWorks to my knowledge (different Kernals).


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Opening Items with NX dataset in Solidworks with SWIM

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

The reason I ask is this.

 

In NX, I search for an Item, I find it, it is built in Solidworks, I can add it into an NX assembly.

 

Can't I do the same?

 

Cem

Re: Opening Items with NX dataset in Solidworks with SWIM

Siemens Phenom Siemens Phenom
Siemens Phenom

No. You cannot.  It is a limitation of Solidworks.  It cannot open either NX nor JT files.  You'd have to export a Parasolid file from NX and import it to Solidworks.


Larry Carpenter, P.E.
CAxPLM Architect @ Siemens Molecular Imaging
Past Board Member @ PLM World, Inc,

Re: Opening Items with NX dataset in Solidworks with SWIM

Valued Contributor
Valued Contributor

Hi Cem,

 

Both Randy and Larry are right. You cant open a NX or JT file directly in SW. 

Here I hope to shed some light on why you can see the SW model when you do a search in NX.

 

I have some cage nuts here as an example. I have master the part in SW and when I saved into my TcRS environment I had the generate JT option turned on.

I then open the the part in NX, but what it did was grab the JT (or you will see MultiCAD in the list). So the 1st feature in the NX feature navigator is the JT_ASSOCIATIVE_BODY.

 

This really great, because if I change the SW part, all I have to do in NX is use the update button in the Displayed Properties window to have the part update in NX as well.

 

2015-11-06_12-50-58.jpg

2015-11-06_13-23-40.jpg