Cancel
Showing results for 
Search instead for 
Did you mean: 

Options and Variants dictionary

Siemens Creator Siemens Creator
Siemens Creator

Hello

 

I am trying to configure a Options and Variants Dictionary in TC10, and i can not find the way!

 

I have looked in the documentation, and i have found that it should be created in the Product Configuration module, and seems quite simple, just file--> new--> dictionary...

 

But in my installation there is no option under file menu!!! (Just close and exit)

 

is needed something to be installed (applications via TEM or templates) in order that this works?

 

I am using a dba user

 

Kind Regards

 

Angel Romero

4 REPLIES

Re: Options and Variants dictionary

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Hello Angel,

 

What Teamcenter version you are using? Tc10.0 or Tc10.1.0 or Tc10.1.2 or later?

Have you installed Product Configurator application? How?

Regards,
Yashodhan

Re: Options and Variants dictionary

Siemens Creator Siemens Creator
Siemens Creator

Hello Yashodaan

 

I am using TC10.1.3, and i think that i have it installes from the TEM

 

Kind Regards

 

Angel Romero

Re: Options and Variants dictionary

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

For Tc10.1.3, could you confirm if you have installed 4G Design or PMM ? 

The Product Configurator is not individually installable. It comes along with above applications.

Search for Application Perspective as "Product Configurator" in Window->Open Perspective

Regards,
Yashodhan

Re: Options and Variants dictionary

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Hello Angel,

 

I would like to know what application you are using 4G Designer or Product Master Management?

During installation of TEM did you select 4G Designer application?

 

In Tc10.1.3 Product Configurator is available only if you choose one of above applications in the TEM. After installation try to do "Window->Open Perspective->Product Configurator" in Teamcenter RAC.

 

Thanks,

Yashodhan

Regards,
Yashodhan