Cancel
Showing results for 
Search instead for 
Did you mean: 

Options to uninstall 2T clients using silent script?

Valued Contributor
Valued Contributor

Dear All,

 

Is there any option to uninstall 2T & 4T TC clients from user machines using silent installer? I do not find this option in tem and in the documents.

 

It looks like the only option is to delete the 2T & 4T client directory from user workstations. 

 

Please suggest if any one of you have any other smart solutions.

 

Thanks

RS

6 REPLIES 6

Re: Options to uninstall 2T clients using silent script?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

The Tc11.3 help files has a section on uninstalling clients here: https://docs.plm.automation.siemens.com/tdoc/tc/11.3/help/#uid:xid1256814:index_client_win:id256661:...

Arden Bedell | Teamcenter Wonk | Applied CAx, LLC

Re: Options to uninstall 2T clients using silent script?

Valued Contributor
Valued Contributor

Dear Arden,

Thanks, but these steps are using the tem.bat. I am looking for a silent mode or alternative modes that will uninstall TC from all user machines without manual intervention.

Any pointers?

 

Regards,

Rajesh

Re: Options to uninstall 2T clients using silent script?

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
Hire an intern?

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Options to uninstall 2T clients using silent script?

Siemens Phenom Siemens Phenom
Siemens Phenom

Yes.  I have done at least a couple presentations on this topic at the annual PLM World conference over the years and provided sample scripts to go with the presentations.  Go to Deploying Clients via Batch Scripting (2016 version) or Deploying NX, I-DEAS, & Teamcenter Via Silent Install Scripts (2011 version).

 

 


Larry Carpenter, P.E.
CAxPLM Architect @ Siemens Molecular Imaging
Past Board Member @ PLM World, Inc,

Re: Options to uninstall 2T clients using silent script?

Valued Contributor
Valued Contributor

Dear Larry,

This was very informative. Thanks so much. Infact, we just figured the same Windows option last week after some research and have started on the same lines for uninstall - your presentation will make it more easier for us as a reference.

Thanks again!!!

 

RS

 

Re: Options to uninstall 2T clients using silent script?

Creator
Creator

Hi,

 

If you are using OTW, you can cerate and custom icd to run otwuninstall.bat and push it.

so that the moment users run portal.bat it will first uninstall the client

 

you can also implement the uninstallation and upgrade using the same consept, this is helpful if there is any upgrade of client done and we want to implemtn it without any manual steps.