Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Over the web full visualization

Gears Phenom Gears Phenom
Gears Phenom

Good afternoon AnnaKroger do you have access to Solution Center?

http://solutions.industrysoftware.automation.siemens.com/

If yes, look for a document with ID: janssend_101017

Re: Over the web full visualization

Legend
Legend

@AnnaKroger

 

Any logs created in \vispoolmanager\jetty\logs folder?

 

You can also give a try with @ArthurRM link to solution document.

Regards
Rafa

Re: Over the web full visualization

Creator
Creator

@ArthurRM
Thanks I've found many related posts in Solution Center and tried some configurations.

@Rafa2
Thanks for your response, after configuring the log4net I wasn't able to see the IISAssignerlog.* in logs folder or any other location. I don't no why this file is not created.

But Finally in poolmanager logs I got this error:

[Thread-440 | WARN  ]: VisServerManager-tcserver:55577:    Reconnection succeeded to VisPoolAssigner-tcserver:55566
[main       | INFO  ]: PoolManager VisServerManager429 starting...
[main       | INFO  ]: java.vm.version: 25.25-b02
[main       | INFO  ]: java.vm.vendor: Oracle Corporation
[main       | INFO  ]: java.vm.info: mixed mode
[main       | INFO  ]: java.io.tmpdir: C:\Program Files\Siemens\Teamcenter11\vispoolmanager\jetty\TEMP\
[main       | INFO  ]: user.name: administrator
[main       | INFO  ]: user.home: C:\Users\Administrator
[main       | INFO  ]: user.dir: C:\Program Files\Siemens\Teamcenter11\vispoolmanager\jetty
[qtp1555690610-21 | ERROR ]: Rejecting assignment
    Class:class com.teamcenter.vis.proxy.ExceptionServerTooFull
    Message:This Vis Server Manager cannot serve more users at this time..
[Thread-445 | INFO  ]: Vis Server Manager is ready!

I cant find any solution to this error.

 

I suspected on graphic card model and driver, is It different than supported cards of TC Visualization?

Re: Over the web full visualization

Legend
Legend

@AnnaKroger

 

This should be a graphic card or driver support issue.

 

Active Workspace is certified and supported on any OEM system that supports graphics cards:

- NVIDIA GRID K1 and K2

- NVIDIA GRID M60

 

Even though you should be able to run Vis Server Manager for evalution process.I had no issues in viewing Solid Edge Sheet metal drawings in AWC (Virtual machine with no graphic card). But if you have the graphic card listed above, I would suggest you to contact GTAC

 

 

Regards
Rafa

Re: Over the web full visualization

Creator
Creator
Thanks @Rafa2 My graphic isn't certified but I didn't think that not works. Are you sure about this error? Is there any way to make sure about the source of error?
Have you any experience with 3d visualization over Thinclient? What plugins should be installed?

Re: Over the web full visualization

Legend
Legend

@AnnaKroger

 

 

I have no experience on 3d visualization over Thinclient.

 

Just compare with my Vis Server manager run, the only difference I see it is rejecting your assignment, might be viewing JT file? The only source is to check with GTAC

 

[qtp1555690610-21 | ERROR ]: Rejecting assignment
    Class:class com.teamcenter.vis.proxy.ExceptionServerTooFull
    Message:This Vis Server Manager cannot serve more users at this time..

image.png

Regards
Rafa

Re: Over the web full visualization

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
Also P40 is certified on newer releases. Some folks are getting away with M10 but not M6 (errors). Keep in mind the usage ass M10 can work for Development (light usage) but not for Production (heavy usage) which will require the bigger GPUs.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4