Showing results for 
Search instead for 
Did you mean: 

PLMXML Export BOM from Seconday Object

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

The goal is to export an specific ItemRevision described on the BOM of an ItemRevision thats attached using an custom relation of another ItemRevision (the original target object).


Currently i have the following lines, but these will only export the BOM if the BOM is attached to the Initialy primary target object.


CLASS.ImanItemLine:TYPE.*Smiley TongueROPERTY.bl_all_child_linesSmiley TongueROCESS+TRAVERSESmiley TongueRIMARY.bl_window_is_BOPWin=="false"

CLASS.ImanItemLine:TYPE.*Smiley TongueROPERTY.bl_revisionSmiley TongueROCESS+TRAVERSE:PRIMARY.bl_window_is_BOPWin=="false"


I have added an line in the closurerule that added the seconday objects to the target. This will add the Seconday object Revision to the export.


CLASS.NG4_ContainerRevision:CLASS.ItemRevision:RelationP2S.NG4_MechanicalRelationSmiley TongueROCESS+TRAVERS


I expected that adding this object to the tagets would result in an export of the BOM But this seems not te be the case any advise?