Cancel
Showing results for 
Search instead for 
Did you mean: 

PLMXML export: XML format

Legend
Legend

Hi All,

 

I have something strange going on with the PLMXML export. The XML-file format is different,with the exact same commandline. I have done some tests and i can reproduce it. Here is the difference:

 

  1. export at commandline: 
    P305412_J_Z9_P_ItemRev_Props__CMD.txt
  2. export with dispatcher running as services: 
    P305412_J_Z9_P_ItemRev_Props__Service.txt

 Files in attachment are XML, but had to rename to post them here.

 

Dispatcher in CMD

commandline.jpg

 

Dispatcher als service:

dispatcher service.jpg

 

 

Any idea what can cause this?

 

Thanks

Fred

 

 

Frederik Verscheure
Evolve Consulting bvba
Freelance NX & Teamcenter consultant
frederik@evolve-consulting.be
5 REPLIES

Re: PLMXML export: XML format

Gears Phenom Gears Phenom
Gears Phenom

When you run it in CMD line, you are using PLMXML export? What does the export look like if you use TCXML export with the same closure rule?

 

Jamie

Re: PLMXML export: XML format

Legend
Legend

The TCXML export gives me a totaly different XML file (PLMXML= 4kB, TCXML=305kB). That is not de correct way to go, i think.

 

Any ideas why the XML-Format is different with the same PLMXML_export command?

Frederik Verscheure
Evolve Consulting bvba
Freelance NX & Teamcenter consultant
frederik@evolve-consulting.be

Re: PLMXML export: XML format

Gears Phenom Gears Phenom
Gears Phenom

TCXML and PLMXML are different XML formats. TCXML will bring more information out about what you are exporting. This is why I asked what it looked like. If it is that much larger, then it isn't why the original files were different. What version of TC?

Re: PLMXML export: XML format

Legend
Legend

TC10.1.2.2

Frederik Verscheure
Evolve Consulting bvba
Freelance NX & Teamcenter consultant
frederik@evolve-consulting.be

Re: PLMXML export: XML format

Siemens Genius Siemens Genius
Siemens Genius
Are the values by any chance localized?

Dispatcher might run in a different localization environment than command line and pick up different values.