01-31-2018 05:53 PM
Hi,
everyone I have this problem
Selected option: Regenerate the schema file
Failed to POM regen schema file: got 515143 error
Failed to POM regen schema file
Error 515143 from POM_install, meaning: POM_unknown_user
*** Caught an error while installing ... aborting!
I run the command install.exe -ayt THE RESULT IS
Site is already installed
I reset password from database and encrypt and modify the tc_profilevars with the same passwor but still showing the same error help me
02-01-2018 01:44 AM - edited 02-01-2018 01:45 AM
Good afternoon, try to check the input for these users in the DBMS, if you use Oracle, then try login using sqplus. Did you run tem.bat as administrator? If not, try to run it again as administrator. You can also try to recreate (delete and create) the database and repeat the installation, make sure that you run the tem.bat with administrator rights.
02-01-2018 09:34 AM
thank you Arthur
I tried again I was importing the database
and my error was the user and password for login into teamcenter, it taken the user and password of old database.
Saludos,