Cancel
Showing results for 
Search instead for 
Did you mean: 

Participant in the an AWC create stylesheet

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hello guys,

 

I had a quick question about the participant and the stylesheet. Is it possible to add the choice of a participant, for a Change Item for exemple, at the creation ?

I tried by adding <property name="revision:Analyst" /> on the  Cm1ProblemReportCreate.

I showed me the participant but when using the add button, it was showing item instead of users.

Do you have any idea how I could make this work, or if I simply can't ?

 

Thank you in advance.

 

Best regards,

 

Benjamin

3 REPLIES

Re: Participant in the an AWC create stylesheet

Legend
Legend

Dear Benjamin,

 

As participants are internally managed using relation (HasParticipant).

I really doubt if partcipant selection can be configured in the create stylesheet either from RAC or AWC.

 

Regards,

Mahendra

Re: Participant in the an AWC create stylesheet

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

It was my guess too but I wasn't sure.

 

Thank you for the help Mahendra :)

Re: Participant in the an AWC create stylesheet

Valued Contributor
Valued Contributor

We did some customizing for defining the participants in change Management. For every project there are different Participants defined in the Project. There is 1 Change Specialist, one Analyst etc defined per Project. The moment the Project is assigned to the Change Objects, the code will define all the Participants defined on the Change Object for this project.