Cancel
Showing results for 
Search instead for 
Did you mean: 

Patching TC Rapid Start from 11.2.0 -> 11.2.2

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hello,

 

How does one properly perform an update process from a base 11.2.0 rapid start installation to 11.2.2?

 

Is it by performing the normal patch process? (extract files from  *_install.zip and replace in tc_root, run patched TEM and update etc., continue to do the same to update the RAC etc.) or is there another way? I haven't been able to find the correct steps in the Siemens documentation.

 

Thank you.

2 REPLIES

Re: Patching TC Rapid Start from 11.2.0 -> 11.2.2

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

The documentation lists it at https://docs.plm.automation.siemens.com/tdoc/tc/11.2.2/help/#uid:xid599308

"To update Teamcenter Rapid Start with the latest service pack or patch, follow the same steps as for installing Teamcenter patches." 

 

--Pat

 

Patrick (Pat) Kennedy, Sr. PLM Application Engineer, Acuity Solutions

Re: Patching TC Rapid Start from 11.2.0 -> 11.2.2

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Thanks, I must have missed that! It worked fine when first installing 11.2.0 and then updating to 11.2.2 using the usual steps. Smiley Happy