Cancel
Showing results for 
Search instead for 
Did you mean: 

Pool Manager - ERROR peer closed connection

Experimenter
Experimenter

Hello,

 

We have 4  entreprise servers on which the requests are dispatched  equaly. After the tc patch (Tc11.2.3.1_0a), the requests are dispatched only for two servers,  even thought  that the pool manager is up on both servers that receive no requests. In the pool log, we got the following message:

WARN - peer closed connection, trying to re-send msg
ERROR - 2nd response to the data failed

 

Some one can give helps ?

 

thank you

 

 

2 REPLIES 2

Re: Pool Manager - ERROR peer closed connection

Valued Contributor
Valued Contributor

can you share the TreeCache configuration that you have defined in insweb.bat while creating the tc.war file?

Re: Pool Manager - ERROR peer closed connection

Experimenter
Experimenter

I resolved this issue  by doing the following actions :

 

 -  telnet host_peeer 17810 

-   start pool manager service

 

Pool manager can't got the right ip address from the peer host, because the peers host is behind a VIP.