Cancel
Showing results for 
Search instead for 
Did you mean: 

Pool Manager settings

Phenom
Phenom

Hi,

 

1. which is the pool manager setting for 4-tier client session timeout ?

 

2.  Is it possible to turn-off the automatic TcServer reassignment from pool manager ? If yes, which is the setting ?

 

Thanks!

11 REPLIES

Re: Pool Manager settings

Phenom
Phenom

I came to know that the settings can be found here: http://server : port/tc/admin/default.aspx.

 

However, this page is not opening due to error: Error 404 - not found, though the pool manager is running.

 

any ideas what could be the problem ?

Re: Pool Manager settings

Siemens Phenom Siemens Phenom
Siemens Phenom

give it a try with http://server:8082

8082 default port 

port can be found in pool_manager\confs\config1\serverPool.properties

Re: Pool Manager settings

Phenom
Phenom

hi @xtof ,

 

Thanks for your answer.

 

the file serverPool.poperties contains only one port called MUX _PORT which is set to 8087. When I tried with this port, I goot following message. Any idea what could be the problem ?

 

HTTP ERROR: 405
Problem accessing /tc/admin/default.aspx. Reason:

HTTP method GET is not supported by this URL

Re: Pool Manager settings

Siemens Phenom Siemens Phenom
Siemens Phenom
There should be an entry JMX_HTTP_ADAPTOR_PORT. MUX_PORT is somehting else...

Re: Pool Manager settings

Phenom
Phenom

 @xtof thanks again! The port was set to 0. After setting it to 8082, I don't see any error. I must however enter login credentials (it says it is from JDMK). I tried infodba, other tc users, windows user of tc-server,webApp server console credentials and none of them worked!

 

Could you please tell what credentials are these ?

 

I am using J2EE Server manager and weblogic app server.

Re: Pool Manager settings

Siemens Phenom Siemens Phenom
Siemens Phenom

login: manager

pwd: manager

Re: Pool Manager settings

Phenom
Phenom

Thanks for quick replies. After these credentials I don't see a login error, but another error: http 400: bad request Smiley Sad

Re: Pool Manager settings

Siemens Phenom Siemens Phenom
Siemens Phenom
Are you sure that the pool manager is running properly on this port?
Last idea is to stop the pool manager, edit the log.properties file and enter a valid path for logging e.g. LogVolumeLocation=c:\\temp\\logs.
After restarting the pool manager have a look at following file: logs\ServerManager\process\ServerManager.log
It should have the following entry: MBean HTML adaptor is configured to start at http://xxx:8082

Re: Pool Manager settings

Phenom
Phenom

I can see this message in command line as well as ServerManager.log as highlighted in the screenshot.

I am also able to login webclient successfully.