Cancel
Showing results for 
Search instead for 
Did you mean: 

Pool Manager startup error

Siemens Creator Siemens Creator
Siemens Creator

While doing mgrstart, I am getting following error. Can anayone help related to this, I need it urgently

 

 

INFO - 2017/11/17-13:21:57.569 UTC - 1069151-uat-tcserver.-719325632 - Using code page UTF-8 for local encoding of service request/response - Teamcenter.SOA.Server
INFO - 2017/11/17-13:21:57.569 UTC - 1069151-uat-tcserver.-719325632 - Listening for requests on pipe:tcserver6@PoolA@2177@1069151-uat-tcserver - Teamcenter.SOA.Server
INFO - 2017/11/17-13:21:57.569 UTC - 1069151-uat-tcserver.-719325632 - Listening for management requests on the same pipe:tcserver6@PoolA@2177@1069151-uat-tcserver - Teamcenter.SOA.Server
INFO - 2017/11/17-13:21:57.571 UTC - 1069151-uat-tcserver.-719325632 - The Transient Volume Root Directory at /usr/siemens/teamcenter/tmp/transientVolume_Administrator already exists. - Teamcenter.Organization.sa at /plm/cynas/tce_iproot5/units/tc11301x_lnx64/src/core/sa/filetickets.cxx(4798)
INFO - 2017/11/17-13:21:57.594 UTC - 1069151-uat-tcserver.-719325632 - Transient volume write access verified using file: /usr/siemens/teamcenter/tmp/transientVolume_Administrator/tvrdtestfile_3532_1510924917 - Teamcenter.Organization.sa at /plm/cynas/tce_iproot5/units/tc11301x_lnx64/src/core/sa/filetickets.cxx(4863)
INFO - 2017/11/17-13:21:57.594 UTC - 1069151-uat-tcserver.-719325632 - The FMS SiteID is -1898923725 - Teamcenter.Organization.sa at /plm/cynas/tce_iproot5/units/tc11301x_lnx64/src/core/sa/filetickets.cxx(1004)
INFO - 2017/11/17-13:21:57.594 UTC - 1069151-uat-tcserver.-719325632 - The Transient Volume Install location is 1069151-uat-tcserver - Teamcenter.Organization.sa at /plm/cynas/tce_iproot5/units/tc11301x_lnx64/src/core/sa/filetickets.cxx(942)
INFO - 2017/11/17-13:21:57.594 UTC - 1069151-uat-tcserver.-719325632 - The Four Tier Transient Volume ID is 0ab36bf1ae64198a3e5b1b4eae8ea253 - Teamcenter.Organization.sa at /plm/cynas/tce_iproot5/units/tc11301x_lnx64/src/core/sa/filetickets.cxx(4091)
INFO - 2017/11/17-13:21:57.594 UTC - 1069151-uat-tcserver.-719325632 - The Transient Volume Root Directory is /usr/siemens/teamcenter/tmp/transientVolume_Administrator - Teamcenter.Organization.sa at /plm/cynas/tce_iproot5/units/tc11301x_lnx64/src/core/sa/filetickets.cxx(1264)
ERROR - 2017/11/17-13:21:57.596 UTC - Thread-139894955439680: - notify_on_sem failed:/PoolA@2177@1069151-uat-tcserver errno=13- Teamcenter.SOA.Tctp
ERROR - 2017/11/17-13:21:57.596 UTC - Thread-139894955439680: - sem_post failure with error 13- Teamcenter.SOA.Tctp
ERROR - 2017/11/17-13:21:57.596 UTC - Thread-139894955439680: - Failed create/connect TcPipe (PoolA@2177@1069151-uat-tcserver/Binding-1)- Teamcenter.SOA.Tctp
ERROR - 2017/11/17-13:21:57.596 UTC - 1069151-uat-tcserver.-719325632 - HeathNotifier: NotifyRequest execute failed. Could not connect to pipe. - Teamcenter.SOA.Server
INFO - 2017/11/17-13:21:57.665 UTC - 1069151-uat-tcserver.-719325632 - Teamcenter Server is ready. - Teamcenter.SOA.tcserver_itk_main
ERROR - 2017/11/17-13:21:57.668 UTC - Thread-139894955439680: - wait_on_sem failed:/tcserver6@PoolA@2177@1069151-uat-tcserver errno=13- Teamcenter.SOA.Tctp
ERROR - 2017/11/17-13:21:57.668 UTC - Thread-139894955439680: - TctpServer failed to accept a TcPipe on the named pipe tcserver6@PoolA@2177@1069151-uat-tcserver. acceptPipe failed- Teamcenter.SOA.Tctp
ERROR - 2017/11/17-13:21:57.668 UTC - Thread-139894955439680: - wait_on_sem failed:/tcserver6@PoolA@2177@1069151-uat-tcserver errno=13- Teamcenter.SOA.Tctp
ERROR - 2017/11/17-13:21:57.668 UTC - Thread-139894955439680: - TctpServer failed to accept a TcPipe on the named pipe tcserver6@PoolA@2177@1069151-uat-tcserver. acceptPipe failed- Teamcenter.SOA.Tctp
ERROR - 2017/11/17-13:21:57.668 UTC - Thread-139894955439680: - wait_on_sem failed:/tcserver6@PoolA@2177@1069151-uat-tcserver errno=13- Teamcenter.SOA.Tctp
ERROR - 2017/11/17-13:21:57.668 UTC - Thread-139894955439680: - TctpServer failed to accept a TcPipe on the named pipe tcserver6@PoolA@2177@1069151-uat-tcserver. acceptPipe failed- Teamcenter.SOA.Tctp

3 REPLIES

Re: Pool Manager startup error

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Obviously Tc11.3.0.1 isn't being run on Windows. What operating system are you using? The error appears to be related to semaphores.

Another possible issue is that you're using the default UTF-8 (docs state) ...
"Before installing Teamcenter on Linux operating systems, ensure that the system is operating in the ISO8859-1 mode, rather than the default UTF-8 mode."

Are you running a database on the same server? Which DB (oracle)?

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Pool Manager startup error

Siemens Creator Siemens Creator
Siemens Creator

we are using amazon RDS for oracle database. which is separete machine

Re: Pool Manager startup error

Siemens Creator Siemens Creator
Siemens Creator
Thanks for reply,I have tried everything what u have said but no luck still shows same error
There is one twist pool manager starts fine with root user but it doesn't work with local user(non root user) which we have used for installation of TC.