Cancel
Showing results for 
Search instead for 
Did you mean: 

Portal.bat disappeared I need your help

Valued Contributor
Valued Contributor

Today when I try to login in to TC, there is not portal.bat.

I don't know what happend.

 

When I try to use TEN to install TC, I got one error.

The error is "". 

 

Someone please could you tell me how to fix the error.

I check FMS_HOME variable and I reboot the PC.

But it is not working.

 

3 REPLIES

Re: Portal.bat disappeared I need your help

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Can you copy portal.bat from another installation? However, TEM not launching is not a good sign. Sounds like a virus scanner did a real number on your installation. It may be faster to trash the whole directory and reinstall it.

UNLESS, this is your server! You weren't too clear about where this portal.bat is/was exactly.

I've also seen this behavior with Windows security patches. If they have been done then roll them back.

Keep us posted.


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11.0.1.mp01 | SW 2016 | TcUA 11.2.3
Evaluating:AW 3.2

Re: Portal.bat disappeared I need your help

Valued Contributor
Valued Contributor

I had to re-install the TC as any necessary file was deleted automatically.

When I login to Client PC, Windows Recovery System was started. But After few minitues, the erros message showed up and it said "The failure of Windows Recovery System ".

 

Also I needed to deleted all the file from registry editor on Windows to fix this error.

This is what I did.

 

 

Re: Portal.bat disappeared I need your help

Esteemed Contributor
Esteemed Contributor

"Windows System Recovery" is the worst thing available, never use it or let it run automatically.

I have never had any benefit from using it, it was always worse after using it.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.0, FBM, MRL 3.1.4 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 10.1
Development: VB.NET, Tcl/Tk    Testing: NX12.0

How to Get the Most from Your Signature in the Community