Cancel
Showing results for 
Search instead for 
Did you mean: 

Preventing data to be exported outside of TC

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Hi guys,

I have a prospect askimg this:
No one would be allowed to download an NX part, EXCEL file or PDF via "right click - named references - download"
There is a manager, users need to ask for a permission from him and then be able to do this.
Anyone done something like that?
It is to protect their data.

They also don't want the NX users to export any data from NX.
How can we do that?

Cem
8 REPLIES

Re: Preventing data to be exported outside of TC

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Anyone on how to restrict users exporting, downloading data from Teamcenter?

 

Cem

Re: Preventing data to be exported outside of TC

Solution Partner Honored Contributor Solution Partner Honored Contributor
Solution Partner Honored Contributor

While you can restrict users from downloading directly from Named References by removing the Export privledge in reality this request is not possible. Especially given that the user may need to download the file to work on it once "permission" is given by the manager. Maybe something can be done in a workflow that changes the permission and allows the user to work on it however that only covers one "download" use-case. For instance, Documents loaded in Viewer are actually downloaded. Basically you have to trust your users at some point.


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Preventing data to be exported outside of TC

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
So you're telling that basically the "Export" in the ACL prevents them to download files from Named References, am I correct?


Saygılarımla,

Cem ALPAY, Yönetici
ÜÇGEN YAZILIM LTD. ŞTİ.
TEL: 0216 550 52 06

[cid:image001.jpg@01D15860.480A6300]

Re: Preventing data to be exported outside of TC

Solution Partner Honored Contributor Solution Partner Honored Contributor
Solution Partner Honored Contributor

Yes. And you can break Teamcenter by using it incorrectly. And it doesn't prevent them from downloading in other areas of Teamcenter. Users are creative so be extra careful.


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Preventing data to be exported outside of TC

Siemens Phenom Siemens Phenom
Siemens Phenom

The only sure fire way to prevent people from somehow taking data is to use a remote terminal (e.g. blade type workstation) for them to log into and work from their PC.  This prevents them, even if they downloaded/exported Teamcenter data on the remote terminal, from getting it to themselves. About the only thing they can do is take screenshots, but if you are worried about that then they shouldn't have access to the data at all.


Larry Carpenter, P.E.
CAxPLM Architect @ Siemens Molecular Imaging
Past Board Member @ PLM World, Inc,

Re: Preventing data to be exported outside of TC

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Actually their manager is just thinking of a permission based idea for exporting.
No one to be allowed to take any data outside, but they might ask permission from their manager and if he grants, than that's ok.
Can a workflow do that?

Saygılarımla,

Cem ALPAY, Yönetici
ÜÇGEN YAZILIM LTD. ŞTİ.
TEL: 0216 550 52 06

[cid:image001.jpg@01D15862.A8FC6E90]

Re: Preventing data to be exported outside of TC

Legend
Legend

That might be even harder to do.

 

Just about the only sure/safe/secure way to prevent your users from exporting data outside of Teamcenter is to deny them read access to the data ;-)

---

Thanks and Regards

Yogesh Fegade

Re: Preventing data to be exported outside of TC

Siemens Phenom Siemens Phenom
Siemens Phenom

Sure. You can have WF temporarily change permissions, and WF can also do the exporting.


Larry Carpenter, P.E.
CAxPLM Architect @ Siemens Molecular Imaging
Past Board Member @ PLM World, Inc,