Cancel
Showing results for 
Search instead for 
Did you mean: 

Project ACL - I cannnot add the user.

Valued Contributor
Valued Contributor

Hi, I have a question,

In the project ACL, I cannnot add the user to the new created project ACL.

I can add infodba, but new created user cannot be added to the new project. Actually new created users was not displayed in the project application.

 

 

And if I add the role to the created project, I cannot create the project ACL.(If I click the creation button, the project was not created.)

 

Could you tell me how to add the new created user to the projects. The problem is that I cannot select user as in the project application there is no user selection area.

2 REPLIES 2

Re: Project ACL - I cannnot add the user.

Valued Contributor
Valued Contributor
Actually if I search the user directly from the search engine, I can add the user to the project. But the assigned the user as well as normal user are not displayed in the project application.
Is this OOTB behavior?

Re: Project ACL - I cannnot add the user.

Valued Contributor
Valued Contributor

Could you be more clear on what operation you are trying to perform here.

 

Did you add users in a specific project, but they are not saved after you close the project application?

 

Or the users got added in the project, however you are not able to define project level ACL using the newly added users?

 

 

 

Swapnil Gawas
Testing, Teamcenter 11.2.x | Active Workspace 3.x