Cancel
Showing results for 
Search instead for 
Did you mean: 

Project ID and Project Name attributes for IRDC form.

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hello ,

I preapared a IRDC form in BMIDE.When Document item is created , Project Manag. Form is attached to created item automatically. Then , i want to fill some areas according to the created item's attributes such as project id and project name. But i couldn't see them as a property . I added the some properties succesfully such as item id -name and revision.How can i add the project information to IRDC form. ?

 

1-) İtem and IRDC form :

2018-08-31_11h41_02.png

2-)Project Yonetim Plani Configurations operation.

I add new custom property as "Project Name " and select exchange direction to "Teamcenter to file". Then i select related or referenced objects < İtem Revision . However , i can not see the project name in attributes area.

Also this item 000209/A is assigned to PRJ-001/Test (test project).

2018-08-31_11h43_22.png

Thanks for helps

Best Regards

Gurkan