Cancel
Showing results for 
Search instead for 
Did you mean: 

Project Security in Teamcenter 11.3 vs 11.2.3

Experimenter
Experimenter

Recently went from Teamcenter 11.2.3 to 11.3. Noticed that in 11.3 the radio button for setting "Project Security" is no longer available. Has anyone else noticed this issue? Solutions?

Note: With legacy projects all is working but with a new project, users can not create data because our policy is to create all data within a project and we see an error message stating "Project Security for this project has not been set". How to set Project Security with no option in the Project application?

 

Thanks,

Paul Parkin

Roush Teamcenter Admin

1 REPLY 1

Re: Project Security in Teamcenter 11.3 vs 11.2.3

Experimenter
Experimenter

So after a few conversations with GTAC, the only way to have "Project" security is to make sure your project is created or assigned as a "Program". Also any projects that are childeren of the Program will not have "Project Security" assigned unless they too are "Programs".