Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Property Rendering in Thin Client

Experimenter
Experimenter

Hello All,

 

In our TC 11.4 environment, we have 3 custom business objects for which property rendering has been used based on a custom property's value(fv9ArchitectureType). It works fine in Rich Client but not working in Thin Client.

 

Below is the renderer definition of one of the business object.

 

<?xml version="1.0" encoding="UTF-8"?>
<icons Version="1.0">
<propertyMap name="ArchitectureTypeMap">
<item key="Physical" value="Overlay Icon Name.png"/>
</propertyMap>

<primaryIcon source="Source Icon Name.png">
<overlayIcon source="fv9ArchitectureType" mapName="ArchitectureTypeMap"/>
</primaryIcon>
</icons>

 

Can you please specify how to have it working in Thin Client too. Checked GTAC and also documentation with no success.

 

Thanks for your valuable help.'


Regards,

Pradeep

1 REPLY 1

Re: Property Rendering in Thin Client

Solution Partner Honored Contributor Solution Partner Honored Contributor
Solution Partner Honored Contributor
Not everything in RAC is supported in Thin Client and this is far enough on the fringe to not be supported, I don't know for sure. I do know that "status" icons need added to tc.war and a preference set … maybe deploying the icons can help?

Web Client
1. Teamcenter preference (tc9>tc10, change protection scope from "User" to "Site") WEB_status_icons=
a. in_process
b. configured
c. TraceLink
d. AllReleaseStatuses
2. Placed Icons in webapp_root\teamcenter\dhtml\icons. The icons have the same name as the preference entry. They are 16x16.png files.
3. Generated EAR file.
Cold deploy (means: stop all but FSC Master, deploy, restart).

https://docs.plm.automation.siemens.com/tdoc/tc/11.4/help/#uid:id1294879


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4