Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Property to fill a dynamic participant

Siemens Legend Siemens Legend
Siemens Legend

I believe this was raised as an ER 7717750 against 11.2.1.

 

Fnd0ParticipantEligibility constant: Need to evaluate multiple group/role combos

Please enhance the Fnd0ParticipantEligibility property constant. Presently it only evaluates a single group/role combination. We need support for multiple group/role combinations.

 

You'll need to contact GTAC to get the current status, but I've not spotted anything in the release notes so I suspect it's still open.

Re: Property to fill a dynamic participant

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi 

 

Is there a way to render the information in the Stylesheet for the Custom Participants in the same way it appears for the OOTB participants ie; a link displaying combination of group /role/ user  ?

 

 

Ambuj

Re: Property to fill a dynamic participant

Valued Contributor
Valued Contributor

A dynamic Participant is defined in RAC with the option Assign Participants and will be assigned to the Object. 

You should define this option in the Stylesheet of the object. You can check in the workflow if this participant is defined and if not create a DO task with instruction on how to define the participant

 

Some customers want to use the dynamic participant depending on the project. In that case you have to write some customizing. You define a user with a specific role in TC Project and this user will be assigned as the correct particpant to the object

Re: Property to fill a dynamic participant

Valued Contributor
Valued Contributor

Thanks for the info. We did some customizing for defining the participants based on role in project.

I will try this handler also