Cancel
Showing results for 
Search instead for 
Did you mean: 

Questions about Solid Edge Integration (SEEC)

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

1. In SEEC Integration, what is the interface between Teamcenter & Solid Edge ?

    As far as I know, it's not SOA.

 

2. Is there any tool to export Solid Edge data (files & metadata) from Teamcenter ? Is any tool/function provided with SEEC for the same ?

2 REPLIES 2

Re: Questions about Solid Edge Integration (SEEC)

Gears Phenom Gears Phenom
Gears Phenom

1. Not sure as I've never even thought about it. Are you trying to program something using SEEC? I'd think you could get your answer from Gtac.

 

2. To get files and metadata you are best to use TC export with a PLMXML closure rule. I don't think SEEC provides this function for both files and metadata. To just get files out only, you could just get the files from the cache folder after you've opened or downloaded into the cache.

 

Jamie

Jamie Griffis | Teamcenter Architect | Applied CAx, LLC

Re: Questions about Solid Edge Integration (SEEC)

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Thanks @Jamie_Griffis .

 

Regarding my first question, it is no more required as I misunderstood the communication from my lead and was heading in a wrong direction.