Cancel
Showing results for 
Search instead for 
Did you mean: 

RapidStart - JT Viewer not working

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hello everyone,

 

we're trying to get the JT Viewer running for RapidStart 10.1.6. there are no JT Utilities and no embedded visualization options available in the TEM.

 

Any help is appreciated.

 

Thanks

2 REPLIES

Re: RapidStart - JT Viewer not working

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
You may not realize it but TcVis FoundationViewer is installed by default with every Rich Client. Look at PORTAL_ROOT\plugins\FoundationViewer, where PORTAL_ROOT is portal when installed using TEM or rac when installed with OTW. That said, what issue are you having with the Viewer tab? Any screen shots or description of the problem would be helpful.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11.0.1.mp01 | SW 2016 | TcUA 11.2.3
Evaluating:AW 3.2

Re: RapidStart - JT Viewer not working

Solution Partner Creator Solution Partner Creator
Solution Partner Creator
There is an option in NX to generate JT-Files when saving. This option was not set. It is working fine now.
Thanks for helping Randy