Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

ReClassifying

Genius
Genius

Hello;

How I can reclassify the ICO's into a new class. Suppose that the the classification hirarchy is being extended and the ICO's which are classified in a general class need to be distributed into more specific classes. Is there any GUI procedure to do this? I appreciate sharing your experience here.

Thanks.

BR.

7 REPLIES 7

Re: ReClassifying

Siemens Genius Siemens Genius
Siemens Genius

Hi,

 

In case of Active Workspace, you can find the edit button on the ICO tile.

Edit takes you back to the Classifcation hierarchy, choose the desired new class and save your re-classification.

 

~Abhi

Re: ReClassifying

Genius
Genius

Thanks @Abhi_Aklujkar 

Could it be done for a multiple ICO's to more to a target class at once? or it must be done one by one? 

in Rich client it can be done also one at a time!!!!

 

Re: ReClassifying

Siemens Genius Siemens Genius
Siemens Genius
In RAC it is possible to reclassify multiple ICOs at once:
Search the ICOs
Open the Table Tab
Select the desired ICOs
Drag and drop them in the desired Class

HTH

Markus

Re: ReClassifying

Siemens Genius Siemens Genius
Siemens Genius

In Active Workspace you cannot multi-select and reclassify.

 

But you have some cool feature, re-classify one object and then copy the ICO from the "copy" button on the tile then go to search for objects you want to re-classify, go to each object  classification tab one-by-one and you can keep pasting the copied ICO :-)

 

 

Re: ReClassifying

Genius
Genius

@Abhi_Aklujkar @MarkusDietz 

Thank you all friends.

Re: ReClassifying

Genius
Genius

@Abhi_Aklujkar @MarkusDietz 

Is it possible to do classification administration tasks in AWC?

Re: ReClassifying

Siemens Genius Siemens Genius
Siemens Genius

No...Admin tasks are not possible in AW.