Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Releasing a NC Machining Revision

Gears Phenom Gears Phenom
Gears Phenom

I wanted to release and NX CAM template in Teamcenter, to prevent modifications, and saw there was no release option.  I presume because there was no workflow created to release that Item type?

 

CAM_Release.jpg

-Dave
NX 11 | Teamcenter 11 | Windows 8.1
2 REPLIES

Re: Releasing a NC Machining Revision

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
You probably have "CR_allow_alternate_procedures" set to "none". You can change that to "any" or "Assigned". For Assigned you'll also want to declare which workflow should be available...
TC_<object_type>_release_procedure. The <object_type> should be the Item Revision type containing the NX CAM template you want to release. A good candidate is "TCM Released".

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Releasing a NC Machining Revision

Gears Phenom Gears Phenom
Gears Phenom

Thanks @RandyEllsworth

-Dave
NX 11 | Teamcenter 11 | Windows 8.1