Cancel
Showing results for 
Search instead for 
Did you mean: 

Report on end-items and multiple where used

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hi,

One of our customers wants to have the following report. Based on the input of x number of end-items (top-level assemblies) that they want to phase out. They want to create a report that:

  1. shows to the lowest level all the childs of the given top-level assemblies.
  2. Does a where-used on those childs and lists all the top-level assemblies in a sepparate colmn
  3. optionally: marks the top-level assemblies  that where part of the input. This could also be done mannualy afterwards if this is tricky.

I would like to hear:

  1. if such a report is possible.
  2. If customizations are required? or can this be done with OOTB functionalities.
  3. What kind of functionallities are needed, ie; transfer rule, report, etc..

Any other sugestions to tackle this use-case? The customer wants to phase out for example 10 - 40 products and these products each contain 50 - 200 unique parts. doing a manual where-used on all these parts is kind of time consuming :)

 

thanks in advance for any replies!

 

Draft use-case:

20170601_101806_resized.jpg 

 

 

1 REPLY

Re: Report on end-items and multiple where used

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

p.s. if someone is interrested in delevering such a report as a service sent me a mail. I would like to give the end-result back to the community though!