Cancel
Showing results for 
Search instead for 
Did you mean: 

Revise only when ItemRev has status

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hi all,

 

is there a setting/preference with which revise can be done ONLY IF the revision has a status ?

7 REPLIES 7

Re: Revise only when ItemRev has status

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

yes. this can be controlled by setting "max working revisions" in BMIDE. Set to 1 to force users to set release status before revising. 

MaxAllowedWorkRevsForItemCopyRev = 1 on ItemRevision in BMIDE.

Re: Revise only when ItemRev has status

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

@Amol_XPLM : You would like to check on MaturityStatuses Business Object Constant on Item Revision object.

Re: Revise only when ItemRev has status

Solution Partner Legend Solution Partner Legend
Solution Partner Legend
thanks @mortenmoi and @PIKG

Re: Revise only when ItemRev has status

Solution Partner Legend Solution Partner Legend
Solution Partner Legend
Apart from setting MaxAllowedWorkRevsForItemCopyRev = 1, I did following setting mentioned in the documentation. Then it worked.

Ensure that the checkLatestReleased extension is attached to the ITEM_copy_rev operation as a precondition on ItemRevision business objects.

Thanks again for your valuable inputs.

Re: Revise only when ItemRev has status

Creator
Creator

Hello 

 

@Amol_XPLM  @RandyEllsworth 

 

Able to revise child item after making MaxAllowedWorkRevsForItemCopyRev=1 and checkLatestReleased extension for ITEM_copy_rev which we don`t want.

 

Detailed:
we have Item(parent item) under Item we have x, y, z items as child

 

we applied MaxAllowedWorkRevsForItemCopyRev=1 and checkLatestReleased extension for ITEM_copy_rev for Parent its working were i am not able create new revision untill Item is relesed- which we want

 

Also we need same solution for child items x, y, z


we applied MaxAllowedWorkRevsForItemCopyRev=1 and checkLatestReleased extension for ITEM_copy_rev for Item-x (child Item) which is not released. Its not working were i am able create new revision 

 

Re: Revise only when ItemRev has status

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
Can you create a new revision after creating a new ItemX and releasing the first revision? Or does this only happen on legacy ItemX's?

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Revise only when ItemRev has status

Creator
Creator

Hai @RandyEllsworth 

 

I have tested few cases where ITEM as business object and with child item, the checkLatestReleased condition is working but for PART business object the condition checkLatestReleased is not working. Any idea about it ?