Cancel
Showing results for 
Search instead for 
Did you mean: 

SEEC feature package

Hello Team,

 

I have Standalone SolidEdge ST10 which I want to integrate with TC 11.2.3,

I have gone through the SEEC documentation which says for server integration i need to browse its template and then option can be enabled to install.

 

But I am unable to Locate that SEEC feature file in GTAC as well as the Standalone installed package.

can someone guide me through this?

 

Regards,

Ganesh

 

 

4 REPLIES 4

Re: SEEC feature package

Gears Phenom Gears Phenom
Gears Phenom

Good afternoon, i think you must download it (SEEC Adminstrator) from GTAC, read more in this thread:

 

https://community.plm.automation.siemens.com/t5/Teamcenter-Administrators-Forum/Teamcenter-Solide-Ed...

Re: SEEC feature package

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

When i am trying to install SEEC it doesnt show any dialouge

 

 

 

 

SE1.PNG

 

 

 

 

 

 

 

 

 

 

SE2.PNG

Re: SEEC feature package

Gears Phenom Gears Phenom
Gears Phenom

Unfortunately I do not have access to SolidEdge on the GTAC to test this. I think that @GaneshDasmale has installed it and will be able to answer your question.

Re: SEEC feature package

you can directly download SEEC Administrator zip file, which has necessary template in it.

 

and for client integration you will be having options in Solidedge to connect 2t/4t TC, if you have correct license for it.