Cancel
Showing results for 
Search instead for 
Did you mean: 

SEEC on VMware - saving takes too long

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello,

I have experience that Solid Edge with Teamcenter on virtual machine VMware 12 makes strange saving. It takes about 3 minutes to save simple solid edge part into Teamcenter. The CPU activity is for this time almost  100%.

If the SE is running on local machine connecting to virtualized server, it is OK.

If somebody has an idea what can be reason of such long saving, please reply.

 

2 REPLIES 2

Re: SEEC on VMware - saving takes too long

Siemens Genius Siemens Genius
Siemens Genius

Hi,

just general check:

If you can dedicate more RAM in VM settings, it will have any effect on Performance/Task Manager?

Best regards,
Miloslav Weitz, Teamcenter Consultant, Siemens PLM Software Czech Republic
Production: Teamcenter 11.5, NX 12, Geolus 9.1
Development: N/A Testing: Teamcenter 12.2, NX 1863, Geolus 10.0

Re: SEEC on VMware - saving takes too long

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

I did it. I increased dedicated memory.

But it had no effect. The problem is CPU.