Cancel
Showing results for 
Search instead for 
Did you mean: 

SOA Library Generation

Legend
Legend

Hi All,

 

Earlier Compilation/building of SOA code using BMIDE of Teamcenter9.1 version generate two library (Soacore.dll and soacoretypes.dll) but with BMIDE of Teamcenter11.X it generate only one library (Soacore.dll)

 

Any idea why? what will be implications of this on code?

 

Thanks..

6 REPLIES

Re: SOA Library Generation

Phenom
Phenom

Did you check TC11 release notes ? You should get info there, in case it has changed.

 

Re: SOA Library Generation

Legend
Legend

I tried but it didn't help :(

Re: SOA Library Generation

Valued Contributor
Valued Contributor
Hi,

In Teamcenter 11.2.3.1 both dll's are generated. But with a bit different name. Something like libXXXYYY.dll and libXXXYYYtypes.dll.
Is the build succeeds?
In the build log files can you see your custom code files compiled and linked?
Is you're BMIDE build environment set up properly?

This is what I can think of as possible issues.

Br,
ZsCsaba
Software Engineer

Re: SOA Library Generation

Legend
Legend

Capture.PNG

 

We do not have the xxxtypes.dll either, but we are not using .NET

Maybe it is only needed for .NET client bindings

 

Re: SOA Library Generation

Legend
Legend

Yes BMIDE env is setup properly and build also successful. Surprisingly code is working fine with Teamcenter without type.dll also.

Re: SOA Library Generation

Legend
Legend

Yes I think that could be valid statement that it required .NET binding. Earlier with Teamcenter9.1 I do have selected those and with Tc11.2 we dont.