Showing results for 
Search instead for 
Did you mean: 

SOARuntimeException - No response received


Hi there

I have got this error on thinclient and 4-tier richclient. "...SOARuntimeException - No response received!"

Server is on .Net webtier and 4-tier. Server manager is working properly (Admin url works with pools in running state).

Actually I'm sure that the problem is not related to firewall or port conflict (Checked). Also there was not any change in IIS application pools.

So I got confused about the problem after reading log files.


Webtier nnnnn.log:

Teamcenter.Presentation.Framework.Authentication.CommonLoginManager [(null)] - 81149.Anonymous.00001 - Login failed for user: infodba; Message is: tcserver2@8085@TCSERVER@4756: No response received.
Teamcenter.WebIntegrations.SOA.SOAAuthFailureResponseHandler [(null)] - 81149.Anonymous.00001 - In SOAAuthFailureResponseHandler:RemoteException/UnknownException occured
Teamcenter.WebIntegrations.Webclient.WebClientPreProcess [(null)] - ::1.90450.Anonymous.00001 - In WebClientPreProcess.
Teamcenter.Presentation.Framework.Authentication.CommonLoginManager [(null)] - ::1.90450.Anonymous.00001 - Login failed for user: infodba; Message is: tcserver4@8085@TCSERVER@4756: No response received.

RAC nnnnn.log:

ERROR tcserver2@8085@TCSERVER@4756: No response received.: tcserver2@8085@TCSERVER@4756: No response received.
com.teamcenter.soa.client.SoaRuntimeException: tcserver2@8085@TCSERVER@4756: No response received.
    at com.teamcenter.rac.kernel.SoaExceptionHandler.handleException(Unknown Source)
    at com.teamcenter.soa.internal.client.XmlRestSender.invoke2(Unknown Source)
    at Source)
    at com.teamcenter.rac.kernel.TCSession.startTCSession(Unknown Source)
    at com.teamcenter.rac.kernel.TCSession.login(Unknown Source)
    at Source)

Could anyone help me please. Is there any other log file that should be read.




Re: SOARuntimeException - No response received

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Check the RAC log: C:\Users\<username>\Teamcenter\RAC\<datetime>\<username>_TcRac_<instancedatetime>.log
The RAC log captures communication between the rich application client (RAC) and the server (tcserver).

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 12 | SW 2017 | Creo 4 | TcUA 11.4
Evaluating:AW 3.4

Re: SOARuntimeException - No response received


Thanks Randy.

The second log is the RAC log file.