Cancel
Showing results for 
Search instead for 
Did you mean: 

SWIM: Attribute mapping to ICS

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hello

 

Is it possible to create within swim a attribute mapping to classification ics?

 

If yes, how the syntax should look like?

 

Thanks for any advice!

 

 

5 REPLIES 5

Re: SWIM: Attribute mapping to ICS

Siemens Genius Siemens Genius
Siemens Genius

Hello,

 

mapping today is limited to the item, item revision, dataset, and any attached forms.  This woudl not include classification ICs.  We would need an enhancement request for tracking this requirement.

 

Thank,

Paul

Re: SWIM: Attribute mapping to ICS

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer
Thank you Paul!

Re: SWIM: Attribute mapping to ICS

Gears Phenom Gears Phenom
Gears Phenom

I did not use SWIM. I do not think this is possible directly. But I think it is possible if you first map the attribute to an object (for example, a revision), and from the ico object you can make a reference to the attribute of the object

Re: SWIM: Attribute mapping to ICS

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
Expanding @ArthurRM suggestion, we mapped an NX attribute to a Classification value using:
{ Dataset type="UGMASTER"
"DB_PART_NAME" : Item.object_name /write_once /description="Part Name"
"DB_PART_DESC" : Item.object_desc /write_once /description="Part Description"

{ Item type="C4_Design"
"NX_Weight" : ItemRevision.c4_Weight /master=cad /allow_null_value /description="c4_Weight"
"NX_Mass" : ItemRevision.ICS(1062) /allow_null_value /description="1062"
}
}

The /allow_null_value switch was critical in case the ItemRevision hadn't been classified yet.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: SWIM: Attribute mapping to ICS

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hello Randy

 

Thank you for your reply. I did this before with NX aswell.

 

According Paul this is not yet supported within SWIM.

 

I opened an ER.