Cancel
Showing results for 
Search instead for 
Did you mean: 

SWIM template installation error

Builder
Builder

Hi there,

 

During the template installation of SWIM11.4.2 on TC 11.4 I got this error:

 

515035: The input string is too long.

After many investigation on log files, finally I've found this explanation:

 

 

515035: The input string is too long. - ERROR: 515035 ERROR MSG: The input string is too long.. - Teamcenter.main at D:\workdir\tc1140x_win64\src\core\main\bmide_manage_templates_itk_main.cxx(435)

 

Actually such kind of errors are new for me.I found a few thing about error 515035 in solution center.

Have you any information about the cause or the solution?

 

Thanks a lot

5 REPLIES

Re: SWIM template installation error

Phenom
Phenom

Hi,

as the only thing you can control is the location of the media, and the fact it says "string to long"... maybe this suggests that the path to your media might have a long folder name or multiple folders with long names?

 

Rich

Richard Bennett
PLM Consultant
www.ProspectPLM.co.uk

Re: SWIM template installation error

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

I have the same issue but with tc 11.4.7. + EDA model.

Looking for soution too.

 

@sma

 

Can you try to regen pom schema?

install -regen_schema_file -u=infodba -p=infodba -g=dba

 

 

It should not work too.

Re: SWIM template installation error

Solution Partner Genius Solution Partner Genius
Solution Partner Genius
Ok. I just find out that clearlocks -assert_all_dead command clear "too long string value:)"
Tem is running fine after this;)

Re: SWIM template installation error

Builder
Builder

@MichalGrygonis wrote:
Ok. I just find out that clearlocks -assert_all_dead command clear "too long string value:)"
Tem is running fine after this;)

Thanks @MichalGrygonis

Are you sure that your problem has fixed?  by just clearlocks? Can you deploy any other BMIDE templates now?

I've tried clearlocks many times but nothing changed. TEM installation process will stop in same progress percent by 515035 again and again.

Re: SWIM template installation error

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Run this SQL statement if you can:

I should return empty result.

SELECT vuid FROM POM_F_LOCK WHERE vuid NOT IN (SELECT vuid FROM POM_R_LOCK WHERE type= 2) ORDER BY vuid 

I can add any template I want.

In my case I had 2 environemts with the same behavior 11.4.0.7 and 11.4.0.6. (utf-8 db's). Both unlocked with clearlocks.