Cancel
Showing results for 
Search instead for 
Did you mean: 

Save Session Structure Manager

Experimenter
Experimenter

Hi All,

 

I try to activate the function in the Structure Manager (TC 11):

File→Save Session

 

Here is the information from the help:

By default, you cannot save a session file. To enable saving of sessions, set the enableSessionFile entry in your customer.properties file to true. If this file does not already  exist, you should create it.

 

I created the file (s. attached) and placed it in the folder: ...portal\plugins\configuration_11000.2.0 

But the function does not come. Some ideas?

 

Thanks, Alex

2 REPLIES 2

Re: Save Session Structure Manager

Solution Partner Honored Contributor Solution Partner Honored Contributor
Solution Partner Honored Contributor
Did you run genregxml after modify the plugins folder *.properties contents (see 001-3049110)? There are several PR's about this setting for a range of Tc versions. Even ownership of the *.pses file can cause issues (see PR 1919078).

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Highlighted

Re: Save Session Structure Manager

Experimenter
Experimenter

Randy, thanks, it works now!