Cancel
Showing results for 
Search instead for 
Did you mean: 

Script error while accessing quick search from Solid Edge(SEEC) - Embedded AWC

Legend
Legend

Hi Experts,

 

I see a script error while user trying to open any file from quick search SEEC 

 

1. Has embedded Active workspace

2. Java version - 1.8.0_162

 

If you say "yes" to the below error it allows to work, Is anyone here came across such error?

 

There is nothing written in TALL logs about this error, Is that soemthing to do with Active  workspace?

 

Capture.PNG

Regards
Rafa
2 REPLIES 2

Re: Script error while accessing quick search from Solid Edge(SEEC) - Embedded AWC

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
Yes, it is AW. Send this to GTAC and they can help resolve the scripting error.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Script error while accessing quick search from Solid Edge(SEEC) - Embedded AWC

Legend
Legend

Thanks Randy!!

 

I will check with GTAC

Regards
Rafa