Cancel
Showing results for 
Search instead for 
Did you mean: 

Searching for attributes in Teamcenter

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi guys,

 

Suppose I have an attribute the user defines in NX. Like "Material = Steel"

Also this attribute is mapped to Teamcenter and I can see it in the Summary tab in Teamcenter Rich Client.

 

Can I make a search based on the attribute "Material" ?

Suppose I want to search for all items that are "steel"

 

Or all items which are produced for a specific customer with a defined attribute called "CustomerName"

 

Cem

3 REPLIES

Re: Searching for attributes in Teamcenter

Valued Contributor
Valued Contributor

Hello Cem,

 

You cannot perform attribute based query with OOTB system defined queries.

 

To perform such search operations, you have to build custom queries using query builder module.

 

For more details kindly find attached link:

 

http://teamcenterplm.blogspot.in/2013/08/teamcenter-query-builder.html

Swapnil Gawas
Testing, Teamcenter 11.2.x | Active Workspace 3.x

Re: Searching for attributes in Teamcenter

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
So also Teamcenter Search can not be used to search for attributes right?


Cem ALPAY
Üçgen Yazılım Ltd. Şti.

--Mobil cihazımdan gönderildi--
--------------------------------

Re: Searching for attributes in Teamcenter

Valued Contributor
Valued Contributor

You cannot search Item attributes using search in Teamcenter. However, you can create a query with

Search class = Item ( if the attribute "steel" is attached to Item properties form).

 

Swapnil Gawas
Testing, Teamcenter 11.2.x | Active Workspace 3.x