Cancel
Showing results for 
Search instead for 
Did you mean: 

Setting assembly imprecise after revising

Experimenter
Experimenter

Hi!

Is there any way (without a workflow or toggle precise/imprecise) to switch an released, precise assembly to imprecise after revising? Our engineering work imprecise on Working parts, then the assembly structure gets released via workflow which sets the structure precise. The next revison should be imprecise again. ATM if we revise via TC or NX the BOM remains precise.

 

Thanks & BR

Bernhard

6 REPLIES 6

Re: Setting assembly imprecise after revising

Experimenter
Experimenter

Ok i found the answer myself, but like a few other things it's of course not working.

My TC Version : 10.1.3 & NX 10

I'm going to report this to GTAC now

 

Maybe someone of you can use it in newer Versions :)

Pls see snapshot for the preference

BR

 

Re: Setting assembly imprecise after revising

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

I need this to, but not in an NX context. Tried this preference, but the next revision was still precise.

 

Anyone know if this is possible when revising a precise structure revision in Active Workspace / Teamcenter. We want the uprev from the precise structure to be imprecise.

Re: Setting assembly imprecise after revising

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
It's just a toggle. You need it to be automatic?

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Highlighted

Re: Setting assembly imprecise after revising

Solution Partner Creator Solution Partner Creator
Solution Partner Creator
Randy - thanks for answering!

Correct. Toggle is the current ‘workaround’. Would like it to be set as imprecise automatically when revised.

If not an OOTB preference, could some BMIDE config solve this? Post-action handler on item revision object?

Any thoughts on this?

Re: Setting assembly imprecise after revising

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
The Teamcenter preferences are an all-or-nothing thing (see TC_config_rule_name). You might be able to set a post-action on create, revise, save-as to toggle the BOM to imprecise but I'm not familiar with how to do it.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Setting assembly imprecise after revising

Genius
Genius

Bernhard

 

We would like to do samething, While revise/saveas, we want assy to be converted to imprecise automatically from precise, Also When we release, Assy needs to be converted to precise.

 

Please let me know, if Anyone has done or if you know how to do