Cancel
Showing results for 
Search instead for 
Did you mean: 

Setting the preference to show default view for Embedded Viewer

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi guys,

 

When I select an object in Teamcenter, in the Viewer tab, I see something previewed.

Can I make sure that the DirectModel is the preferred one if there are more than one object that could be displayed by the Viewer?

As you see below, there is a PDF and a JT model but PDF is displayed first.

I always want the 3D model to be shown first.

2015-06-25_15-34-22.jpg

 

Thanks!

 

Cem