Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Setup Thin Client to open CGM directly in standalone TC Vis Base

Experimenter
Experimenter

Hello,

 

I'm trying to launch the standalone TC Vis Base directly from the thin client to open 2D drawing data stored in the UGMASTER CGM.

 

The current procedure is to open the UGMASTER and download the PRT and then open in TC Vis Base, but we want to avoid, if possible, downloading the files.

 

When trying to open the item (UGMASTER with CGM data or Direct Model with JT file) via View->Teamcenter Visualization, the following error appears:

 

image.png

I have the following preferences set up:

 

  • VMU_Datasets, with the default values plus UGPART and UGMASTER.
  • VMU_FileSearchOrder, with the default values plus UGPART and UGMASTER.
  • VMU_RelationSearchOrder, with the default values.
  • WEB_EnableVisualization, 1
  • WEB_EnablePSEVisualization, 1
  • TC_show_open_in_vmu_button, true

 

I also have a rich client install in the machine I'm working with this. We work with JBOSS service.

 

Is this possible? If not, which is the correct procedure to visualize the 2D drawings in the TC Vis standalone version?

 

Any information missing, please let me know to provide it.

 

Thanks in advance.

ROBERTO RAMÍREZ, Analysis & Tooling engineer, FRISA Forge
Production: NX11.0.2 | TC 11.2.0 | TC Vis Base 11.2
Testing: NX12.0.0 | TC 11.4.0
1 REPLY 1

Re: Setup Thin Client to open CGM directly in standalone TC Vis Base

Experimenter
Experimenter

Hello,

 

Working with GTAC we arrived at the following solution:

 

- Intall de java version for 32-bit (we use JRE7u60, but had installed just the 64-bit version).

- Open the Thin Client in Internet Explorer (supports JAVA Applets), previously working in Chrome.

- Enable the Java permission requested.

 

If the mentioned preferences are correctly set as mentioned above, the Thin Client integration with TC Vis should work fine after this.

 

*Considering a FSC service is installed in the client.

 

Regards.

ROBERTO RAMÍREZ, Analysis & Tooling engineer, FRISA Forge
Production: NX11.0.2 | TC 11.2.0 | TC Vis Base 11.2
Testing: NX12.0.0 | TC 11.4.0