Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid edge variable link with mapped property in TC

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello,

I was asked to link few dimensions from Solid Edge part with Teamcenter property, e.g. length of some kind of parts. The dimensions in SE are controlled by variables. Variable can be exposed, that means writen as custom property. In case I map the property with Teamcenter, SE can not link - expose it.

Has anybody hint or idea how to fix it?

1 REPLY 1

Re: Solid edge variable link with mapped property in TC

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

My fault.

Dimension variable of SE has been incorrectly exposed to TC-attribute of double.

I defined in BM two attributes: one as String, second as Double.

Then I set in SE part scalar variable exposed to attribute Double. Dimension variable has been set by formula and exposed to attribute of Scalar. Now it works nice.