Cancel
Showing results for 
Search instead for 
Did you mean: 

SolidEdge Mass Attribute not seen in File Properties or Property Manager.

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello ,

System Info :

SolidEdge ST10

Teamcenter 11.3

I'm using the SE with integrated of TC. Firstly , i create an item then assign a material from default SE database. I can see the mass result in Teamcenter<MV(Physical Properties) (you can see the picture 1)

Picture :1

2018-06-29_16h37_40.png2018-06-29_16h39_10.png

However , In the property manager < RMB show properties feature , i can not see the property of mass to use in TC. (you can see the pic 2)2018-06-29_16h41_00.png

 

 

How can i add the mass property here or what is the best and rigth way to use mass properties in TC.

Best Regards

Gurkan

 

9 REPLIES

Re: SolidEdge Mass Attribute not seen in File Properties or Property Manager.

Gears Phenom Gears Phenom
Gears Phenom

Can you share your attribute mapping for the SE file types? I'm suspecting it isn't mapped there.

 

Jamie

Jamie Griffis | Teamcenter Architect | Applied CAx, LLC

Re: SolidEdge Mass Attribute not seen in File Properties or Property Manager.

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi Jamie ,

Thanks for fast response.2018-06-29_16h53_11.png Mapping instance is below.

 

 

Re: SolidEdge Mass Attribute not seen in File Properties or Property Manager.

Gears Phenom Gears Phenom
Gears Phenom

Here is how I have it in my mapping:

 

        "MATERIAL" : ItemRevision.m6_Material /master=cad /description="Material"

 

Try adding this mapping and restart SE to see if it shows up.

Jamie Griffis | Teamcenter Architect | Applied CAx, LLC

Re: SolidEdge Mass Attribute not seen in File Properties or Property Manager.

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi Jaime ,

There is no problem with the material value , according to my mapping file it works correctly. That is the point , how should add the mass property ?

 

"Mass" :ItemRevision.******/master=cad/ description="Mass" is it correct ?

 

Re: SolidEdge Mass Attribute not seen in File Properties or Property Manager.

Gears Phenom Gears Phenom
Gears Phenom

Sorry! I copied the wrong line. Oops.

 

        "Mass" : ItemRevision.m6_Mass /master=cad /description="Mass"

Jamie Griffis | Teamcenter Architect | Applied CAx, LLC

Re: SolidEdge Mass Attribute not seen in File Properties or Property Manager.

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Oo not problem , i see :smileyhappy:

So , i think first off all , i should create new variable for mass properties in BMIDE. Then i must arrange the mapping file what you mentioned Like ;

 

"Mass" : ItemRevision.m6_Mass /master=cad /description="Mass"

 

 

Re: SolidEdge Mass Attribute not seen in File Properties or Property Manager.

Gears Phenom Gears Phenom
Gears Phenom

Yes, you'll need a property on your Item Revision to store the info from SE into TC.

Jamie Griffis | Teamcenter Architect | Applied CAx, LLC

Re: SolidEdge Mass Attribute not seen in File Properties or Property Manager.

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Yes , it works correctly thanks a lot for helps :smileyhappy:

I need one more help , how can i add mass property in structure manager. I select the item rev. and send to structure manager , RMB BOM Line to insert new column but i couldn't see the mass attribute in list. How can i solve it ?

 

Best Regards

Gurkan

Re: SolidEdge Mass Attribute not seen in File Properties or Property Manager.

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

I solved it (Attribute in Structre Manager) thanks a lot for helps.

Best Regards

Gurkan