Cancel
Showing results for 
Search instead for 
Did you mean: 

Specific view error with a profil

Valued Contributor
Valued Contributor

Hi everybody,

 

I have a special issue with one user and I think, one of you can help me.

 

One will explain the case into one item:

 

One user see not correctly the item. Specially he don't see the last open revision. For all others users into my environment, this is ok.

 

I think, the user have a special parameter on preferences but I don't found which! Can you help me? Or perhaps with the command line preferences_manager, I can clean him profil. I test with the

preferences_manager -mode=clear

but no effect.

 

Thank you

PLM Technical IT
3 REPLIES

Re: Specific view error with a profil

Siemens Phenom Siemens Phenom
Siemens Phenom

looks more like an access issue. Please check in the ACL control list if the user has read access on the working revision. 

xtof

Re: Specific view error with a profil

Valued Contributor
Valued Contributor

Thank you for your idea but He have the same access like other users.

 

Have you other idea?

 

 

PLM Technical IT

Re: Specific view error with a profil

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

I also believe this is an ACL but if you want to pursue the preferences route then export and clear the users preferences using:

preferences_manager -u=infodba -p=infodba -g=dba -mode=export -scope=USER -target=username -out_file=C:\Temp\username.xml

Then delete them using:

 

preferences_manager -u=infodba -p=infodba -g=dba -mode=remove -scope=USER -target=username

You can control which preferences are deleted by supplying a file listing each pref on a separate line using "-file=deletetheseprefs.txt".

 


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11.0.1.mp01 | SW 2016 | TcUA 11.2.3
Evaluating:AW 3.2