Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Start NX from within Teamcenter

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

As you can see the title I fail to run NX with Teamcenter connection.

 

Teamcenter is running as normal.

I have set all the (I think so) the parameters in the bats.

 

start_nxmanager.bat

and also in the

tc_nx120tcin.bat I have set the parameters

 

but now I am confused how I have to start nx, I mean with which command?

 

%UGII_BASE_DIR%\UGII\ugs_router -ug

NX starts in native mode no connection

 

%UGII_BASE_DIR%\UGII\ugs_router -ugm

(it fails: user and password)

 

In the end I want NX with Teamcenter connection no active workspace.

 

How do I start NX with Teamcenter connection?

 

 

And:

Managed mode = active workspace?

Teamcenter integration in NX = active workspace?

2 REPLIES 2

Re: Start NX from within Teamcenter

Gears Phenom Gears Phenom
Gears Phenom

Re: Start NX from within Teamcenter

Solution Partner Honored Contributor Solution Partner Honored Contributor
Solution Partner Honored Contributor
The readme in NX120custom describes the modifications to start_nxmanager.bat that need to happen. Basically you have to declare the location for NX custom (set NX_CUSTOM_DIR=T:\NX120custom) then the launch script (%NX_CUSTOM_DIR%\Tc_NX110TCIN.bat %*).

The process: Launch Teamcenter (portal.bat), make sure nothing is selected (hit ESC) and click the NX button. This calls start_nxmanager.bat which you know about from above.

Setting NX_CUSTOM_DIR can be a UNC path to the NXcustom folder shared on the network but not all things behave when using the UNC method (\\server\share\NX120custom). I prefer to use a mapped drive common in the company like T:\ and map it to the shared folder. The batch scripts in NXcustom like the mapped drive method.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4