Cancel
Showing results for 
Search instead for 
Did you mean: 

Status flags

Honored Contributor
Honored Contributor

Using NX9 and TC 10

 

How would you go about changing the flags for the different status?  currently a checkered flag shows for released, inactive, and obsolete.

 

Note, I am not a TC admin, I'd just like to present some "go here, do this" to our admin.

 

Also, can you make it impossible to add a component that is obsolete or inactive, to an assembly in NX?  or at least pop up a warning?

 

Thanks,

 Dave

-Dave
NX1867(if it had versions) | Teamcenter 11.6 | Windows 10
17 REPLIES 17

Re: Status flags

Genius
Genius

Dave,

 

You can certainly add a custom icon for the each status type. For which, Your admin has to do the following things.

 

1) Create an custom icon based on the different status (It should be 16 x16 pixels and in PNG Format)

2) Right click on the status type in BMIDE and add the icons to project.

3) Deploy the template.

4) Have to create a custom configuration file add to each rich client installation manually and reset the registry / create a .jar file add it to the OTW Script.

 

Secondly, I am not sure if we could get a warning. But with the access manager you can restrict to see the obsolete revisions of the items from the view and searching. That way one cannot add it to the assembly.

 

Hope this helps!

Cheers.

 

 

 

 

 

Teamcenter 10.1.7
TC Visualization 10.1.7
NX:11.02 | NX 9.02 | Catia V5 R2012 | AutoCAD 2018 | In-Context Editor |

Re: Status flags

Honored Contributor
Honored Contributor

Thanks!

 

I suspect there are other OOTB flags, like the checkered flag?  red, yellow, etc.

-Dave
NX1867(if it had versions) | Teamcenter 11.6 | Windows 10

Re: Status flags

Creator
Creator

Hello,

 

I would request you to check \\portal\plugins folder for the jar file for icons.

If not available then create one as written below:

com."Prefixname".icons_"version".0."revision".jar

 

it should contain com\teamcenter\rac\common folder create a folder icon and copy paste your png files.

create a 'common_user.properties' file which should contain these 2 lines for every status

 

release_status_list.'Name'.ICON=icon/'NAME'.png
release_statuses.'NAME'.ICON=icon/'NAME'.png

 

after the jar file is updated. Start TC Prompt and commit portal\registry\'name'.bat file

 

make sure while using TC Prompt all the processes regarding the Teamcenter are killed.

 

Hope this might help you.

 

Re: Status flags

Experimenter
Experimenter
Hello,

Can any one please explain in short what what it exactly means of different color of flag.

like green color means released.

Re: Status flags

Gears Genius Gears Genius
Gears Genius

In respect to Rapid Start releases the colours are:

 

Red (90)          Obsolete

Green (60)      Released

Blue (30)         Development

Grey (20)        Reviewed

Black (10)       Rejected

 

There is also:

 

Magenta (40)

DarkGreen (50)

DarkYellow (70)

Orange (80)

Re: Status flags

Pioneer
Pioneer

Hi Expert,

 

I tried using below but it is not working.

release_statuses.'NAME'.ICON=icon/'NAME'.png

Any sugesstion on this ?

Re: Status flags

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor

Make sure you use the Display Name and not the System Name. Escape any spaces.
Production\ Release

release_status_list.Tooling\ As\ Built\ Release.ICON=images/ACME4toolflag.png
release_statuses.Tooling\ As\ Built\ Release.ICON=images/ACME4toolflag.png


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Status flags

Pioneer
Pioneer

Hi Randy Ellsworth,

 

Thank you for your valuable suggestion.

I am using OOTB status (Rejected), and in this case system name and display name both are same.

I am able to append custom status icon next to IR but i want to change under IR too.

Note: I am trying to achive this in TC 8.3.6 environment using eclipse plugin project.

 

Thanks,

Indra

Re: Status flags

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
portal\plugins\configuration_11000.2.0\images\ff0000flag.png
PNG must be 16x16

portal\plugins\configuration_11000.2.0\customer.properties:
# Release status objects
# Next to ItemRevision - use release_status_list format
# Under ItemRevision - use release_statuses format
# Example (USE DISPLAY NAME)
release_status_list.Blue\ Flame.ICON=images/ff0000flag.png
release_statuses.Blue\ Flame.ICON=images/ff0000flag.png

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4