Cancel
Showing results for 
Search instead for 
Did you mean: 

Structure Manager is not Working

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi, is there a reason so that Structure Manager won’t start?

In NX the saving failed with this notification: (original is in german) An error occurred while importing the PLMXML document to the arrangement occurence in Teamcenter.

Any ideas how can I solve this?

Thx in advance

2 REPLIES
Highlighted

Re: Structure Manager is not Working

Solution Partner Honored Contributor Solution Partner Honored Contributor
Solution Partner Honored Contributor
Usually means you have an Item Revision in the structure that has an illegal char. It doesn't know how to process it so shows nothing. Review the tcserver syslog to identify the ItemRev then go fix the name/description. Once completed, structure manager will display the BOM correctly.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Structure Manager is not Working

Genius
Genius

Hi,

 

Faced similar issue that structure manager is not working when I installed the feature NX integration and the corresponding NX DLLS which are in the corporate server TC_ROOT/bin were not copied to the pool manager TC_ROOT/bin.

 

may be if you have similar architecture, can give a try.

 

Thanks

Phani