Cancel
Showing results for 
Search instead for 
Did you mean: 

Synchronous Dispatcher connection error

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hello,

 

I create a schedule, inside it I create a task.
when right click on task I select "launch to workflow" I got below error message :

"Synchronous Dispatcher connection error: The Teamcenter server is having
difficulties connecting to the Synchronous Dispatcher. Please contact your
site administrator.
Error when launching the Workflow process on the task.
Error when launching the Workflow process on the task.
Error when launching the Workflow process on the task."

I already up the services for Dispatcher,Moduler and Scheduler but getting the same error if go through the same process.

Teamcenter Version 8.3

Windows Server

 

thanks,

1 REPLY

Re: Synchronous Dispatcher connection error

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

This means the Dispatcher Client is having issues. The key word in the error is "connecting". (see IR6346772).


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11.0.1.mp01 | SW 2016 | TcUA 11.2.3
Evaluating:AW 3.2